DRV.EMUEPULSEWIDTH

Description

EMU Encoder Out PulseClosedWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated Width Register

Sets pulse width for CW/CCW and Step and Direction modes. This parameter does not effect the A quad B mode. To calculate emuOutPulseWidth:

(Desired pulse width -40 nsec)/520 nsec

Requirement DSFPGA-03-306
Bits Bits Description
11:0 emuOutPulseWidth Read/Write
12 bit unsigned number minimum resolution is 520 nsec.
Reset state – 0
15:12   reserved
  • Register is in counts (12 bit)
  • Register * 520ns + 40ns is the actual pulse with.
  • Register = 1 = pulse width is 560ns = 0.56us (minimum value)
  • For each register increment the pulse width is raised by 0.52us

Example

50 usecs pulse width

emuOutPulseWidth = (50 usecs – 40 nsec)/520 nsec = 96

actual pulse = 96*520 nsec + 40 nsec = 49.88 usecs.

General Information

Type

TBD

Units

us(microseconds)

Range

4.08 us to 2621.48 us

Default Value

4.08 us

Data Type

Float

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

520Dh/0

M_01-00-00-000

Related Topics

DRV.EMUEMODE