DRV.EMUESTEPCMDPOUT
Description
This parameter is the denominator in the scaling factor for DRV.EMUSTEPCMD.
The internal stepper command is calculated as follows:
General Information
Type |
R/W |
Units |
N/A |
Range |
-65536 to 65536 |
Default Value |
65536 |
Data Type |
Integer |
Start Version |
M_01-14-03-000 |
Related Topics
Stepper Control and EEOs over fieldbus