DRV.FAULTDISPLAYMODE

Description

DRV.FAULTDISPLAYMODE sets the LED display behavior when faults are present.

Value Description
0 Only the highest priority fault is displayed.
1 All faults displayed.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-13-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

53C7h

M_01-13-00-000

Related Topics

DRV.CLRFAULTS , DRV.FAULTHIST, DRV.CLRFAULTHIST