FAULTx.ACTION

Description

This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.

Parameter Value Drive Action
0 Disable Ampllifier
1 Ignore (fault will not be reported)

General Information

Type

R/W

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-04-16-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5259h/0 FAULT130.ACTION M_01-04-16-000
525Ah/0 FAULT131.ACTION
525Bh/0 FAULT132.ACTION
525Ch/0 FAULT134.ACTION

5267h/0

FAULT451.ACTION
525Dh/0 FAULT702.ACTION