IL.FOLDWTHRESH

Description

ILClosed"Instruction list" This is a low-level language and resembles assembly.FOLDWTHRESH is the warning level of the current foldback algorithm. When IL.IFOLD drops below IL.FOLDWTHRESH a warning is generated.

To ensure that the current foldback warning level is never reached, IL.FOLDWTHRESH should be set well below the continuous current value for both the drive and the motor. You can also set the IL.FOLDFTHRESH value to zero.

General Information

Type

NV Parameter

Units

Arms

Range

0 to 500 Arms

Default Value

0 A

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

355Ah/0

M_01-00-00-000

Related Topics

1    Current Loop