IL.VLIMIT

Description

ILClosed"Instruction list" This is a low-level language and resembles assembly.VLIMIT sets the velocity limit for operation in torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.

When set to a non-zero value, the current supplied to the motor will be limited to prevent the drive from accelerating beyond -IL.VLIMIT / IL.VLIMIT.

General Information

Type

NV Parameter

Units

Depends on UNIT.VROTARY or UNIT.VLINEAR

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Linear: counts/s, mm/s, µm/s

Range

Rotary:

0.000 to 15,000.000 rpm

0.000 to 250.000 rps

0.000 to 90,000.000 deg/s

0.000 to 1,250.000 custom units/s

0.000 to 1570.796 rad/s

Linear:

0.000 to 1,073,741,824,000.000 counts/s

0.000 to 250.000*MOTOR.PITCH mm/sec

0.000 to 250,000.000*MOTOR.PITCH µm/s

Default Value

Rotary:

0.000 rpm

0.000 rps

0.000 deg/s

0.000 custom units/s

0.000 rad/s

Linear:

0.000 counts/s

0.000*MOTOR.PITCH mm/sec

0.000 *MOTOR.PITCH µm/sec

Data Type

Float

Start Version

M_01-14-04-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

207Fh/0

M_01-14-04-000

Related Topics

1    Current Loop