MOTOR.FIELDWEAKENING

Description

Allows a surface permanent magnet motor (MOTOR.TYPE = 0) to operate as an interior permanent magnet motor (MOTOR.TYPE = 6).

This keyword can only be set when MOTOR.TYPE = 0. Any other MOTOR.TYPE will result in an error and MOTOR.FIELDWEAKENING will not be applied.

General Information

Type

R/W Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-13-02-000

Related Topics

Motor

MOTOR.TYPE