MOTOR.LQLL

Description

This parameter is used to configure the motor line-to-line inductance.


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.

General Information

Type

NV Parameter

Units

mH

Range

1 to 232 mH

Default Value

17.000 mH

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3455h/0

M_01-00-00-000

Related Topics

Motor