MOTOR.TBRAKEAPP

Description

This parameter is used to configure the mechanical delay required for the motor brake to close. The AKD will servo to hold position for the time set, allowing the brake to apply.


  • If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.

General Information

Type

NV Parameter

Units

ms

Range

0 to 1,000 ms

Default Value

75 ms

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

366Eh/0

M_01-00-00-000

Related Topics

Motor