VL.GENMODE

Description

This parameter is used to select the velocity generator mode.

Mode

Description

0

d/dt mode: The derivative of the mechanical angle of the drive is fed to a first order low pass.

1

Luenberger Observer mode

 

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

51B0h/0

M_01-00-00-000

Related Topics

Velocity Loop