What's Fixed in KAS v3.03

Items fixed by KAS v3.03
Defect Descriotion
BZ-6554 Add Variable window in Dictionary Window is not getting closed when dim of 0 or 1 is selected and clicked on ok
BZ-8655 Multi-dimension cannot be set when adding a variable
BZ-10340 MC_GrpReadCmdVel doesn't report correct value for group velocity when axes group is in e-stop state.
BZ-10370 E22 on simulator with ECATCommErrors function block
BZ-10383 IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger Crashes when opening SoftScope if OpenGLClosedOpenGL (Open Graphics Library) is a standard specification defining a cross-language, cross-platform API for writing applications that produce 2D and 3D computer graphics. The Softscope uses this API to implement graphical manipulations is not supported
BZ-10384 Web-server wheel position value wrong for PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML custom units
BZ-10385 Lower part of main view is cut-off when switching windows
BZ-10407 MC_MoveAbsolute(…) to apply the cumulative Superimposed move distance. For more details, see the MC_AXIS_PARAM_APPLY_SUPERIMPOSED_DISTANCE parameter in: Understanding KAS > Motion Concepts > PLCopen > Axis Parameters
BZ-10412 EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Slave Station Alias EEPROM CRCClosed"Cyclic redundancy check" A CRC is a type of function that takes as input a data stream of any length and produces as output a value of a certain fixed size. The term CRC is often used to denote either the function or the function's output. A CRC can be used as a checksum to detect accidental alteration of data during transmission or storage checksum should include the reserved locations 0x5, 0x6 data. BBH SCU FSoE EtherCAT master has non-zero values in reserved locations, causing EEPROM corruption with KAS IDE versions 3.03.0.80412 (or older).
BZ-10420 IDE-Workbench crash when user variable is selected in WB Scope view
BZ-10421 IDE fails to find zlibwapi.dll if a disconnected network is in the Windows Path
BZ-10422 Velocity compensation factor and filter parameters can not be set for digitizing axes
BZ-10429 Save KAS file from Coordinated motion template is corrupted
BZ-10450 IDE disconnects when IDE-WB Scope view is opened
BZ-10454 Compile error: Create new library
BZ-10455 KAS Simulator crashes When Closing 2nd Instance