Working with the Hardware

In some cases, using the buttons on the controller may be preferable to using the web server. On the front of the controller there are two buttons, B2 and B3. B2 is above B3. These buttons may be used to enter Recovery Mode (see "Booting from the Recovery Image"), Display the IP Address of a PDMM or PCMM, stop and start the application, reset the control to factory settings (see "Reset the Controller to Factory Settings"), and backup/restore the firmware.

Result Press and hold
B2 Recovery Mode
B3 Menu access

Table 6-1: B2/B3 button functionality at start-up

Press Result
B2 Menu option selector
B3 Menu access

Table 6-2: B2/B3 button functionality while running