MLBlkIsReady

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Check if a block is ready.

Input

Input

Data Type

Range

Unit

Default

Description

ID

DINT

-2147483648 to 2147483648

N/A

No default

ID number of a created Pipe Block.

Output

Output

Data Type

Range

Unit

Default

Description

Default (.Q)

BOOL

N/A

N/A

No default

Returns TRUE if no function of a specified Pipe Block is running.

See Function - General Rules for more information.

Remarks

  • Returns TRUE if no function of a specified Pipe Block is running.
  • Returns FALSE if the selected Pipe Block has a function running.

  • Same return value as the .Q output of a specific function itself.

FBD Language

MLBlkIsReady FBD Figure

FFLD Language

MLBlkIsReady LD Figure

ST Language

//Check if the MST Pipe Block named “MASTER” has a function running 
IsReady := MLBlkIsReady( PipeNetwork.MASTER );

See Also