MLCompReadRef

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the reference position of a comparator block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483648

N/A

No default

ID number of an initiated Comparator object.

Outputs

Output

Data Type

Range

Unit

Default

Description

Reference

LREAL

No range

User units

No default

Returns the current reference position of the Comparator object.

Remarks

  • The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
  • The Comparator Transition Flag stays TRUE until it is reset.

FBD Language

MLCompReadRef: FBD example

FFLD Language

MLCompReadRef: LD example

ST Language

//Return the Comparator Reference value
CompRef := MLCompReadRef( PipeNetwork.MyComp );

See Also