MLCompReset

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Clear the Transition Flag of a comparator Pipe Block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483648

N/A

No default

ID number of an initiated Comparator object.

Outputs

Output

Data Type

Range

Unit

Default

Description

Default (.Q)

BOOL

No range

N/A

No default

Returns TRUE when function starts to execute.

See Function - General Rules for more information.

Remarks

  • The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
  • The Comparator Transition Flag stays TRUE until it is reset.

FBD Language

MLCompReset: FBD example

FFLD Language

MLCompReset: LD example

ST Language

//Clear the Transition Flag of a Comparator object
MLCompReset( PipeNetwork.MyComp );

See Also