max

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the maximum of two integers.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1

ANY

 

 

 

First input.

IN2

ANY

 

 

 

Second input.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

IN1 if IN1 > IN2; IN2 otherwise.

Remarks

None

FBD Language

MaxFbd.gif (1257 octets)

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The comparison is executed only if EN is TRUE.
    • ENO has the same value as EN.

MaxLd.gif (1526 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN1
     MAX IN2
     ST  Q    (* Q is the maximum of IN1 and IN2 *)

ST Language

Q := MAX (IN1, IN2);

See Also