mod / modLR / modR

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculation of modulo.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

mod = DINT

modR = REAL

modLR = LREAL

 

 

 

Input value.

BASE

mod = DINT

modR = REAL

modLR = LREAL

 

 

 

Base of the modulo.

Outputs

Output

Data Type

Range

Unit

Description

Q

mod = DINT

modR = REAL

modLR = LREAL

 

 

Modulo: rest of the integer division (IN / BASE).

Remarks

None

FBD Language

ModFbd.gif (1274 octets)

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The comparison is executed only if EN is TRUE.
    • ENO has the same value as EN.

ModLd.gif (1523 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     MOD BASE
     ST  Q    (* Q is the rest of integer division: IN / BASE *)

ST Language

Q := MOD (IN, BASE);

See Also