atan / atanL
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
IN |
REAL / LREAL |
|
|
|
Real value. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
REAL / LREAL |
|
|
Result: arc-tangent of IN. |
Remarks
None
FBD Language
FFLD Language
- In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
- The output rung (ENO) keeps the same value as the input rung.
(* The function is executed only if EN is TRUE. *)
(* ENO keeps the same value as EN. *)
IL Language
- In the IL "Instruction list" This is a low-level language and resembles assembly language, the first input must be loaded before the function call.
Op1: LD "Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
ATAN
ST Q (* Q is: ATAN (IN) *)
ST Language
Q := ATAN (IN);
See Also