tan / tanL

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculate a tangent.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL / LREAL

 

 

 

Real value.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL / LREAL

 

 

Result: Tangent of IN.

Remarks

None

FBD Language

TanFbd.gif (1141 octets)

FFLD Language

  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
  • The function is executed only if EN is TRUE.
  • ENO keeps the same value as EN.

TanLd.gif (1403 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     TAN
     ST  Q    (* Q is: TAN (IN) *)

ST Language

Q := TAN (IN);

See Also