delete

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Delete characters in a string.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

STRING

 

 

 

Character string.

NBC

DINT

 

 

 

Number of characters to be deleted.

POS

DINT

 

 

 

Position of the first deleted character.

The first character position is 1.

Outputs

Output

Data Type

Range

Unit

Description

Q

STRING

 

 

Modified string.

Remarks

  • The first valid character position is 1.

FBD Language

DeleteFbd.gif (1386 octets)

FFLD Language

  • In the FFLD language, the conversion is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.

DeleteLd.gif (1637 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them     IN
     DELETE NBC, POS
     ST     Q

ST Language

Q := DELETE (IN, NBC, POS);

See Also