REPLACEPLCopen motion icon

FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Replace characters in a string.

Inputs

Inputs

Data Type

Description

IN

STRING

Character string.

STR

STRING

String containing the characters to be inserted in place of NDEL removed characters.

NDEL

DINT

Number of characters to be deleted before insertion of STR.

POS

DINT

Position where characters are replaced (first character position is 1).

Outputs

Output Data Type Description

Q

STRING

Modified string.

Remarks

  • The first valid character position is 1.
  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
  • In the ILClosed "Instruction list" This is a low-level language and resembles assembly language, the first input (the string) must be loaded in the current result before calling the function.
    • Other arguments are operands of the function separated by comas.

ST Language

Q := REPLACE (IN, STR, NDEL, POS);

FBD Language

ReplaceFbd.gif (1540 octets)

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
ReplaceLd.gif (1762 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them      IN
     REPLACE STR, NDEL, POS
     ST      Q

See Also