ror

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Rotate bits of a register to the right.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Register.

NBR

ANY

 

 

 

Number of rotations (each rotation is 1 bit).

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

Rotated register.

Remarks

  • Arguments can be signed or unsigned integers from 8- to 32-bits.

Diagram

RorDiag.gif (1373 octets)

FBD Language

RorFbd.gif (1241 octets)

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The rotation is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     ROR NBR
     ST  Q

ST Language

Q := ROR (IN, NBR);

See Also