shl

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Shift bits of a register to the left.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Register.

NBS

ANY

 

 

 

Number of shifts (each shift is 1 bit).

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

Shifted register.

Remarks

  • Arguments can be signed or unsigned integers from 8- to 32-bits.

Diagram

ShlDiag.gif (1297 octets)

FBD Language

ShlFbd.gif (1252 octets)

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The shift is executed only if EN is TRUE.
    • ENO has the same value as EN.

ShlLd.gif (1508 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     SHL NBS
     ST Q

ST Language

Q := SHL (IN, NBS);

See Also