ACTION#.SOURCE

Description

This keyword defines the input source for an action.

Value Name Description Signal Type
0 No source Default value of no specified source N?A
1 Mains ready This digital source goes high when the bus voltage is available to the drive. It does not take any ID or parameters. Digital
2 Digital Input This digital source corresponds to a DIN. It takes an ID. Digital
3 Digital DIO (Bidirectional) This digital source corresponds to DIO. It takes an ID. Digital
4 Velocity Feedback This analog source holds the value of AXIS#.VL.FB. It takes an axis ID. Analog
5 Axis Faulted This digital source goes high when a fault exists on an axis. It takes an axis ID. Digital
6 Home Complete This digital source is high when a Home operation is completed on an axis. It takes an axis ID. Digital
7 Motion Task in Position This digital source is high when on an axis specified by the axis ID, a MotionTask specified by Source Parameter, has reached its position. It takes both ID and parameter. Digital
8 Controlled Stop Active This digital source is high when a Controlled Stop is active on an axis. It takes an axis ID. Digital
9 Software Limit This digital source is high when a software limit on an axis is reached. It takes an axis ID. Digital
10 MT Not Running This digital source is high if, on the axis specified by the source ID, either the Motion Task specified by the source parameter has stopped running (i.e. AXIS#.MT.RUNNING for that task went from 1 to 0) or, if the source parameter is set to -1, all Motion Tasks have stopped running (i.e. AXIS#.MT.RUNNINGTASK went from any other value to -1). This source does not check whether the actual position has reached the Motion Task’s target position. Digital
11 Position Error, Absolute This analog source holds the value of AXIS#.PL.ERR . It takes an axis ID. Analog
12 Axis Enabled This digital source holds the value of AXIS#.ACTIVE . It takes an axis ID. Digital
13 Analog Input This analog source holds the value of AIN#.VALUE. It takes as Source ID, the ID of AIN. Analog
14 Current Command This analog source holds the value of AXIS#.IL.CMD. It takes an axis ID. Analog
15 Velocity Error This analog source holds the value of AXIS#.VL.ERR. It takes an axis ID. Analog
16 Velocity Command This analog source holds the value of AXIS#.VL.CMD. It takes an axis ID. Analog
17 Position Feedback This analog source holds the value AXIS#.PL.FB. It takes an axis ID. Analog
18 Axis Disable Immediately This digital source goes High if the axis disables when a fault is generated with a fault reaction of either “Disable power stage” or “Dynamic braking”. Refer to the Reaction column in Faults and Warning Messages for more information. Digital
19 Brake State This digital source holds the value of BRAKE#.STATE. It takes a Brake ID. Digital
20 Ready to Operate (RTO/BTB) This digital source goes High when the drive/axis is ready to operate, i.e., the power stage is ready and there are no axis faults. It can default to an ID of 0 for the entire drive or take an axis ID. Digital
21 Compare Digital Inputs This bit-mapped source shows the value of all the DINs and DIOs compared with a mask which is settable with UI. See Action Source 21 - Compare Digital Outputs for more information. Digital
22 Feedback Fault This source holds the value of FB#.FAULTS. It takes a Feedback ID. Digital
23 User Variable This source holds the value of USER.INT#. It takes an ID. Analog
24 Action Row Running This digital source indicates if an Action Row is running, i.e. if the task is being executed (see ACTION.RUNNING). It takes an Action Row ID. Digital
25 Current Feedback This analog source holds the value of AXIS#.IL.FB . It takes an axis ID. Analog
26 Recordable Parameter This allows an action to be triggered by using any Recordable Parameter. When selected, the Source Text window now accepts an array parameter keyword and index. See Action Source 26 - Recordable Parameter for more information. Analog
27 Drive Initialized This digital source goes high when the drive has finished initialization after booting. Digital
28 Move Complete This digital source is high if, on the axis specified by the source ID, either the motion task specified by the source parameter has stopped running (i.e. AXIS#.MT.RUNNING for that task went from 1 to 0) and the actual position is within AXIS#.SETTLE.P around the motion task’s target position or, if the source parameter is set to -1, all motion tasks have stopped running (i.e. AXIS#.MT.RUNNINGTASK went from any other value to -1) and the actual position is within AXIS#.SETTLE.P around the last motion task’s target position. It will only go low when the motion task is started again, not if the actual position is no longer within AXIS#.SETTLE.P around the target position. Digital
29 Ready To Enable This digital source goes High when the drive/axis is ready to enable and all disable sources are off (except software enable), i.e., the power stage is ready and there are no axis faults. It can default to an ID of 0 for the entire drive or take an axis ID. Digital
200 Safe Input This digital source holds the value of a SIN (Safety Digital Input). It takes the SIN ID. Digital
201 Safe Dual Input This digital source holds the value of a DUAL (Dual Safety Digital Input). It takes the SIN DUAL ID. Digital
202 Safe Output This digital source holds the value of a SOUT (Safety Digital Output). It takes the SOUT ID. Digital
203 Safe Dual Output This digital source holds the value of a SOUT DUAL (Dual Safety Digital Output). It takes the SOUT DUAL ID. Digital
204 STO Active This digital source holds the value of STO Active. It takes an Axis ID. Digital
205 SS1 Active This digital source holds the value of SS1 Active. It takes an Axis ID and an Instance ID. Digital
206 SS2 Active This digital source holds the value of SS2 Active. It takes an Axis ID and an Instance ID. Digital
207 SOS Active This digital source holds the value of SOS Active. It takes an Axis ID and an Instance ID. Digital
208 SBC Active This digital source holds the value of SBC Active. It takes an Axis ID. Digital
209 SLS Active This digital source holds the value of SLS Active. It takes an Axis ID and an Instance ID. Digital
210 SSM in Range This digital source holds the value of SSM in Range. It takes an Axis ID and an Instance ID. Digital
211 SSR Active This digital source holds the value of SSR Active. It takes an Axis ID and an Instance ID. Digital
212 SDIn in Motion This digital source holds the value of SDIn in Motion. It takes an Axis ID. Digital
213 SDIp in Motion This digital source holds the value of SDIp in Motion. It takes an Axis ID. Digital
214 SLA Active This digital source holds the value of SLA Active. It takes an Axis ID. Digital
215 SAR Active This digital source holds the value of SAR Active. It takes an Axis ID and an Instance ID. Digital
216 SLI Active This digital source holds the value of SLI Active. It takes an Axis ID and an Instance ID. Digital
217 SLP Active This digital source holds the value of SLP Active. It takes an Axis ID and an Instance ID. Digital
218 SCA in Range This digital source holds the value of SCA in Range. It takes an Axis ID and an Instance ID. Digital

26 – Recordable Parameter

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 28 and 200 to 218

Default Value

0 (no source)

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.SOURCE

3904h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.SOURCE

3904h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.SOURCE

3904h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.SOURCE

3904h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.SOURCE

3904h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.SOURCE

3904h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.SOURCE

3904h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.SOURCE

3904h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.SOURCE

3904h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.SOURCE

3904h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.SOURCE

3904h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.SOURCE

3904h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.SOURCE

3904h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.SOURCE

3904h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.SOURCE

3904h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.SOURCE

3904h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.SOURCE

3904h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.SOURCE

3904h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.SOURCE

3904h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.SOURCE

3904h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.SOURCE

3904h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.SOURCE

3904h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.SOURCE

3904h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.SOURCE

3904h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.SOURCE

3904h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.SOURCE

3904h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.SOURCE

3904h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.SOURCE

3904h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.SOURCE

3904h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.SOURCE

3904h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.SOURCE

3904h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.SOURCE

3904h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40500

1

40500 (0x9e34)

ACTION1.SOURCE

Unsigned8

Read/Write

Yes

40501

1

40501 (0x9e35)

ACTION2.SOURCE

Unsigned8

Read/Write

Yes

40502

1

40502 (0x9e36)

ACTION3.SOURCE

Unsigned8

Read/Write

Yes

40503

1

40503 (0x9e37)

ACTION4.SOURCE

Unsigned8

Read/Write

Yes

40504

1

40504 (0x9e38)

ACTION5.SOURCE

Unsigned8

Read/Write

Yes

40505

1

40505 (0x9e39)

ACTION6.SOURCE

Unsigned8

Read/Write

Yes

40506

1

40506 (0x9e3a)

ACTION7.SOURCE

Unsigned8

Read/Write

Yes

40507

1

40507 (0x9e3b)

ACTION8.SOURCE

Unsigned8

Read/Write

Yes

40508

1

40508 (0x9e3c)

ACTION9.SOURCE

Unsigned8

Read/Write

Yes

40509

1

40509 (0x9e3d)

ACTION10.SOURCE

Unsigned8

Read/Write

Yes

40510

1

40510 (0x9e3e)

ACTION11.SOURCE

Unsigned8

Read/Write

Yes

40511

1

40511 (0x9e3f)

ACTION12.SOURCE

Unsigned8

Read/Write

Yes

40512

1

40512 (0x9e40)

ACTION13.SOURCE

Unsigned8

Read/Write

Yes

40513

1

40513 (0x9e41)

ACTION14.SOURCE

Unsigned8

Read/Write

Yes

40514

1

40514 (0x9e42)

ACTION15.SOURCE

Unsigned8

Read/Write

Yes

40515

1

40515 (0x9e43)

ACTION16.SOURCE

Unsigned8

Read/Write

Yes

40516

1

40516 (0x9e44)

ACTION17.SOURCE

Unsigned8

Read/Write

Yes

40517

1

40517 (0x9e45)

ACTION18.SOURCE

Unsigned8

Read/Write

Yes

40518

1

40518 (0x9e46)

ACTION19.SOURCE

Unsigned8

Read/Write

Yes

40519

1

40519 (0x9e47)

ACTION20.SOURCE

Unsigned8

Read/Write

Yes

40520

1

40520 (0x9e48)

ACTION21.SOURCE

Unsigned8

Read/Write

Yes

40521

1

40521 (0x9e49)

ACTION22.SOURCE

Unsigned8

Read/Write

Yes

40522

1

40522 (0x9e4a)

ACTION23.SOURCE

Unsigned8

Read/Write

Yes

40523

1

40523 (0x9e4b)

ACTION24.SOURCE

Unsigned8

Read/Write

Yes

40524

1

40524 (0x9e4c)

ACTION25.SOURCE

Unsigned8

Read/Write

Yes

40525

1

40525 (0x9e4d)

ACTION26.SOURCE

Unsigned8

Read/Write

Yes

40526

1

40526 (0x9e4e)

ACTION27.SOURCE

Unsigned8

Read/Write

Yes

40527

1

40527 (0x9e4f)

ACTION28.SOURCE

Unsigned8

Read/Write

Yes

40528

1

40528 (0x9e50)

ACTION29.SOURCE

Unsigned8

Read/Write

Yes

40529

1

40529 (0x9e51)

ACTION30.SOURCE

Unsigned8

Read/Write

Yes

40530

1

40530 (0x9e52)

ACTION31.SOURCE

Unsigned8

Read/Write

Yes

40531

1

40531 (0x9e53)

ACTION32.SOURCE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.SOURCE

40500

Unsigned8

Read/Write

-

ACTION2.SOURCE

40501

Unsigned8

Read/Write

-

ACTION3.SOURCE

40502

Unsigned8

Read/Write

-

ACTION4.SOURCE

40503

Unsigned8

Read/Write

-

ACTION5.SOURCE

40504

Unsigned8

Read/Write

-

ACTION6.SOURCE

40505

Unsigned8

Read/Write

-

ACTION7.SOURCE

40506

Unsigned8

Read/Write

-

ACTION8.SOURCE

40507

Unsigned8

Read/Write

-

ACTION9.SOURCE

40508

Unsigned8

Read/Write

-

ACTION10.SOURCE

40509

Unsigned8

Read/Write

-

ACTION11.SOURCE

40510

Unsigned8

Read/Write

-

ACTION12.SOURCE

40511

Unsigned8

Read/Write

-

ACTION13.SOURCE

40512

Unsigned8

Read/Write

-

ACTION14.SOURCE

40513

Unsigned8

Read/Write

-

ACTION15.SOURCE

40514

Unsigned8

Read/Write

-

ACTION16.SOURCE

40515

Unsigned8

Read/Write

-

ACTION17.SOURCE

40516

Unsigned8

Read/Write

-

ACTION18.SOURCE

40517

Unsigned8

Read/Write

-

ACTION19.SOURCE

40518

Unsigned8

Read/Write

-

ACTION20.SOURCE

40519

Unsigned8

Read/Write

-

ACTION21.SOURCE

40520

Unsigned8

Read/Write

-

ACTION22.SOURCE

40521

Unsigned8

Read/Write

-

ACTION23.SOURCE

40522

Unsigned8

Read/Write

-

ACTION24.SOURCE

40523

Unsigned8

Read/Write

-

ACTION25.SOURCE

40524

Unsigned8

Read/Write

-

ACTION26.SOURCE

40525

Unsigned8

Read/Write

-

ACTION27.SOURCE

40526

Unsigned8

Read/Write

-

ACTION28.SOURCE

40527

Unsigned8

Read/Write

-

ACTION29.SOURCE

40528

Unsigned8

Read/Write

-

ACTION30.SOURCE

40529

Unsigned8

Read/Write

-

ACTION31.SOURCE

40530

Unsigned8

Read/Write

-

ACTION32.SOURCE

40531

Unsigned8

Read/Write

-