AXIS#.CANOPEN.CONTROLBIT##.MODE
Description
This parameter is used to set a mode to the specified bit in the DS402 control word (AXIS#.CANOPEN.CONTROLWORD, Controlword Object 6040h). This allows the user to select different functions for Controlword bits 11-15.
| Mode | Name | Description |
|---|---|---|
| 0 | None | Control bit ignored |
| 1 | MODPDIR |
Bit value 0 sets AXIS#.PL.MODPDIR = 1 (positive) Bit value 1 sets AXIS#.PL.MODPDIR = 2 (negative) |
-
- If multiple bits in the control word are set to the same mode, the upper bit value overrides the lower bit value.
Examples
Code
Setting bit 11 in the control word to MODPDIR mode:
-->AXIS1.CANOPEN.CONTROLBIT11.MODE 1 -->AXIS1.CANOPEN.CONTROLWORD (control word set via PDO) 0x31 -->AXIS1.PL.MODPDIR 1 -->AXIS1.CANOPEN.CONTROLWORD (control word set via PDO) 0x8031 -->AXIS1.PL.MODPDIR 2
Context
6040h, 6840h Controlword - AxisX
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-01-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range |
0- None 1 - MODPDIR mode |
| Default Value | 0 (None) |
| Data Type | Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
EtherCAT and CAN drives: AKD2G-SPC/AKD2G-SPE
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.CANOPEN.CONTROLBIT11.MODE |
5003h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS1.CANOPEN.CONTROLBIT12.MODE |
5003h |
0bh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS1.CANOPEN.CONTROLBIT13.MODE |
5003h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS1.CANOPEN.CONTROLBIT14.MODE |
5003h |
0dh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS1.CANOPEN.CONTROLBIT15.MODE |
5003h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.CANOPEN.CONTROLBIT11.MODE |
5103h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.CANOPEN.CONTROLBIT12.MODE |
5103h |
0bh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.CANOPEN.CONTROLBIT13.MODE |
5103h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.CANOPEN.CONTROLBIT14.MODE |
5103h |
0dh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.CANOPEN.CONTROLBIT15.MODE |
5103h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |