AXIS#.HOME.CREEPFACTOR

Description

AXIS#.HOME.CREEPFACTOR is the percentage of the homing speed (AXIS#.HOME.V) used when searching for the feedback’s index or limit switch. AXIS#.HOME.CREEPFACTOR is only used in home modes 1, 2, 3, 6 and 10.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

%

Range

1 to 100

Default Value

50

Data Type

Integer

See Also

AXIS#.HOME.V, AXIS#.HOME.MODE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.CREEPFACTOR

5008h

0bh

Unsigned32

-

-

Read/Write

No

AXIS2.HOME.CREEPFACTOR

5108h

0bh

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6105

1

6105 (0x17d9)

AXIS1.HOME.CREEPFACTOR

Unsigned32

Read/Write

Yes

71641

2

6105 (0x17d9)

AXIS2.HOME.CREEPFACTOR

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.CREEPFACTOR

6105

Unsigned32

Read/Write

-

Related Topics

Homing