AXIS#.HOME.V

Description

AXIS#.HOME.V is the velocity used while homing. When searching for an index this speed is reduced by AXIS#.HOME.CREEPFACTOR.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

60 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.V

5008h

10h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.HOME.V

5108h

10h

Unsigned32

Velocity

-

Read/Write

No

AXIS1.HOME.V

6099h

01h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.HOME.V

6899h

01h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6112

1

6112 (0x17e0)

AXIS1.HOME.V

Signed32

Read/Write

Yes

71648

2

6112 (0x17e0)

AXIS2.HOME.V

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.V

6112

Float

Read/Write

Velocity

Related Topics

Homing