AXIS#.HOME.IPEAK

Description

AXIS#.HOME.IPEAK is the peak current that will be applied when homing against a mechanical stop.

AXIS#.HOME.IPEAK is used when AXIS#.HOME.MODE is 8, 9, 10 or 12.

The current limits AXIS#.IL.LIMITP and AXIS#.IL.LIMITN are set to ±AXIS#.HOME.IPEAK while homing. Once the home position has been found, the current limits are restored before any additional move using AXIS#.HOME.DIST starts.

By default, this value is zero. For the axis to move AXIS#.HOME.IPEAK needs to be set to greater than zero. If AXIS#.HOME.IPEAK is zero and AXIS#.HOME.MODE is 8, 9 or 10, W6026 warning is generated. If the home move is started with this warning, then F6026 fault is generated.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

Arms

Range

0 to AXIS#.IPEAK

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.MODE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.IPEAK

5008h

05h

Signed32

-

1000:1

Read/Write

No

AXIS2.HOME.IPEAK

5108h

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6106

1

6106 (0x17da)

AXIS1.HOME.IPEAK

Signed32

Read/Write

Yes

71642

2

6106 (0x17da)

AXIS2.HOME.IPEAK

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.IPEAK

6106

Float

Read/Write

-

Related Topics

Homing