AXIS#.IL.COGCOMPH.ENABLE
Description
AXIS#.IL.COGCOMPH.EN can be used to enable / disable the cogging compensation current configured byAXIS#.IL.COGCOMPH.A, AXIS#.IL.COGCOMPH.N, and AXIS#.IL.COGCOMPH.P .
-
- This parameter is automatically configured for some Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if AXIS#.MOTOR.DISAUTOSET index = 1.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-14-02-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.COGCOMPH.ENABLE |
500ah |
2bh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.IL.COGCOMPH.ENABLE |
510ah |
2bh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5870 |
1 |
5870 (0x16ee) |
AXIS1.IL.COGCOMPH.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
71406 |
2 |
5870 (0x16ee) |
AXIS2.IL.COGCOMPH.ENABLE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.COGCOMPH.ENABLE |
5870 |
Unsigned8 |
Read/Write |
- |