AXIS#.MT.V
Description
AXIS#.MT.V specifies the motion task velocity. This is the maximum speed the axis will use when moving to the target position. The axis will accelerate up to this speed and stay at this speed before decelerating to a stop at the desired position. The axis may not get to this speed if the distance is short.
The motion task velocity is also limited by AXIS#.VL.LIMITP or AXIS#.VL.LIMITN depending on the direction of the motion task.
By default AXIS#.MT.V is zero and will generate an error if you try to start the motion task with AXIS#.MT.MOVE. You have to set AXIS#.MT.V to a non-zero value before this motion task can be started.
Examples
Code
Sets the velocity of motion task 0 to 60 RPM. The first parameter is the motion task number and the second is the velocity.
-->AXIS1.MT.V 0 60
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only Array |
|
Units |
Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
0 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MT.V 0 |
50d3h |
01h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 1 |
50d3h |
02h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 2 |
50d3h |
03h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 3 |
50d3h |
04h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 4 |
50d3h |
05h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 5 |
50d3h |
06h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 6 |
50d3h |
07h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 7 |
50d3h |
08h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 8 |
50d3h |
09h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 9 |
50d3h |
0ah |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 10 |
50d3h |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 11 |
50d3h |
0ch |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 12 |
50d3h |
0dh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 13 |
50d3h |
0eh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 14 |
50d3h |
0fh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 15 |
50d3h |
10h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 16 |
50d3h |
11h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 17 |
50d3h |
12h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 18 |
50d3h |
13h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 19 |
50d3h |
14h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 20 |
50d3h |
15h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 21 |
50d3h |
16h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 22 |
50d3h |
17h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 23 |
50d3h |
18h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 24 |
50d3h |
19h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 25 |
50d3h |
1ah |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 26 |
50d3h |
1bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 27 |
50d3h |
1ch |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 28 |
50d3h |
1dh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 29 |
50d3h |
1eh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 30 |
50d3h |
1fh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS1.MT.V 31 |
50d3h |
20h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 0 |
51d3h |
01h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 1 |
51d3h |
02h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 2 |
51d3h |
03h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 3 |
51d3h |
04h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 4 |
51d3h |
05h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 5 |
51d3h |
06h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 6 |
51d3h |
07h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 7 |
51d3h |
08h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 8 |
51d3h |
09h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 9 |
51d3h |
0ah |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 10 |
51d3h |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 11 |
51d3h |
0ch |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 12 |
51d3h |
0dh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 13 |
51d3h |
0eh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 14 |
51d3h |
0fh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 15 |
51d3h |
10h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 16 |
51d3h |
11h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 17 |
51d3h |
12h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 18 |
51d3h |
13h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 19 |
51d3h |
14h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 20 |
51d3h |
15h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 21 |
51d3h |
16h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 22 |
51d3h |
17h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 23 |
51d3h |
18h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 24 |
51d3h |
19h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 25 |
51d3h |
1ah |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 26 |
51d3h |
1bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 27 |
51d3h |
1ch |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 28 |
51d3h |
1dh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 29 |
51d3h |
1eh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 30 |
51d3h |
1fh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MT.V 31 |
51d3h |
20h |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6309 |
1 |
6309 (0x18a5) |
AXIS1.MT.V |
Signed32[32] |
Read/Write |
Yes |
|
71845 |
2 |
6309 (0x18a5) |
AXIS2.MT.V |
Signed32[32] |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MT.V |
6309 |
Float[32] |
Read/Write |
Velocity |
Related Topics