CAP#.P

Description

The captured position. This value only changes when a new position is captured.

Examples

Usage

CAP#.SOURCE Description Units
1-5 FB#.P Same as FB#.P
11-12 AXIS#.PL.FB Same as AXIS#.PL.FB

Code

-->CAP1.P
0.000 [Counts]
-->

Context

See Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units

Depends on CAP#.SOURCE.

See table above to know what the units are.

Range

N/A

Default Value 0
Data Type Float
See Also

CAP#.SOURCE, CAP#.T

Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CAP1.P

4400h

0bh

Signed32

-

1000:1

Read only

No

CAP2.P

4401h

0bh

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31030

1

31030 (0x7936)

CAP1.P

Signed32

Read Only

Yes

31031

1

31031 (0x7937)

CAP2.P

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.P

31030

Signed32

Read Only

Position

CAP2.P

31031

Signed32

Read Only

Position