CAP#.PRESELECT

Description

Selects the digital input used as the precondition input.

Examples

Usage

Value Description

1-12 (2 is the default)

Digital Inputs DIN1 to 12

21 – 26

 

Bidirectional digital inputs. DIO1 to 6

31 – 35

Z-Pulses from feedbacks 1 to 5
41 - 42 Z-pulse from Axis 1 or Axis 2

51 - 52

CMP# output

Not all hardware variants have the hardware to support all of these options. For example, a single axis drive will not support option 42.

Code

-->CAP1.PRESELECT 21
-->

Context

See Capture.

Versions

Action Version Notes
Implemented 02-00-00-000
Added CMP# 02-12-00-000 Added values for CMP# Output

General Information

Type

Read/Write

Units

N/A

Range

1 to 12, 21 to 26, 31 to 35, 41 to 42

Default Value

2

Data Type

Integer

See Also CAP#.PREMODE, CAP#.PREEDGE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CAP1.PRESELECT

4400h

04h

Unsigned8

-

-

Read/Write

No

CAP2.PRESELECT

4401h

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31060

1

31060 (0x7954)

CAP1.PRESELECT

Unsigned8

Read/Write

Yes

31061

1

31061 (0x7955)

CAP2.PRESELECT

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.PRESELECT

31060

Unsigned8

Read/Write

-

CAP2.PRESELECT

31061

Unsigned8

Read/Write

-

Related Topics

Capture

CAP#.TRIGGER