MODBUS.EN
Description
Enables or disables the Modbus interface.
0 = Disabled. All Modbus messages are ignored.
1 = Enabled (default). Modbus messages are managed by the drive.
Example
The following stops any Modbus messages from being processed.
-->MODBUS.EN 0
-->
Context
For more information, see Modbus Installation and Setup.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Read Write Parameter |
|
Units |
N/A |
|
Range |
0 or 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
| See Also | MODBUS.INFO |
|
Stored in Non-Volatile Memory |
Yes |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
MODBUS.EN |
3014h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3702 |
1 |
3702 (0xe76) |
MODBUS.EN |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
MODBUS.EN |
3702 |
Unsigned8 |
Read/Write |
- |