MODBUS.MSGDUMP
Description
MODBUS.MSGDUMP prints any logged Modbus messages. Logging is enabled and disabled using MODBUS.MSGLOG.
The AKD2G drive records the contents of the Modbus messages sent from the drive in addition to the IP address and port number or the remote endpoint. The DRV.RUNTIME is latched at each message and is also recorded and returned by MODBUS.MSGDUMP.
Examples
To enable logging set MODBUS.MSGDUMP to 1.
-->MODBUS.MSGLOG 1 -->
To view the logged messages.
-->MODBUS.MSGDUMP (39d:21h:30m:48s): 1 242 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944 (39d:21h:30m:48s): 1 242 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944 (39d:21h:30m:56s): 1 243 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944 (39d:21h:30m:56s): 1 243 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944 -->
Context
For more information, see Message Logging.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Info Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |