MODBUS.MSGLOG
Description
Use MODBUS.MSGLOG to stop Modbus message logging. If MODBUS.MSGLOG is 1, then the AKD2G drive records all Modbus messages to and from the drive. Logs are shown using MODBUS.MSGDUMP.
The message log is cleared every time the log is enabled, MODBUS.MSGLOG starts from 0 to 1.
The message log can contain a maximum of twenty entries. If the limit of entries is exceeded then older entries are discarded.
|
Value |
Description |
|---|---|
|
0 |
Disabled |
|
1 |
Enabled (default) |
Examples
To enable logging set MODBUS.MSGLOG to 1.
-->MODBUS.MSGLOG 1 -->
To view logged messages.
-->MODBUS.MSGDUMP (39d:21h:30m:48s): 1 242 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944 (39d:21h:30m:48s): 1 242 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944 (39d:21h:30m:56s): 1 243 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944 (39d:21h:30m:56s): 1 243 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944 -->
Context
For more information, see Message Logging.
Versions
| Action | Version | Notes |
|---|---|---|
|
Implemented |
02-05-00-000 |
General Information
|
Type |
Read Write Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
MODBUS.MSGLOG |
3014h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3707 |
1 |
3707 (0xe7b) |
MODBUS.MSGLOG |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
MODBUS.MSGLOG |
3707 |
Unsigned8 |
Read/Write |
- |