AXIS#.SAFE.SBT.MOVE

Description

Executes Safe Brake Test (SBT) on the specified axis. All brakes attached to this axis are tested. A maximum of two brakes can be attached to a specific axis. For this command to work, Safe Brake Control (SBC) and SBT must be configured consistently in the SMM using safety parameters.

Code

--> AXIS1.SAFE.SBT.MOVE

Context

For complete information on SBT, refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.SBT.MOVE

2fc0h

01h

Unsigned32

-

-

Write only

No

AXIS2.SAFE.SBT.MOVE

2fc0h

02h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

10004

1

10004 (0x2714)

AXIS1.SAFE.SBT.MOVE

Unsigned8

Read/Write

No

75540

2

10004 (0x2714)

AXIS2.SAFE.SBT.MOVE

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SAFE.SBT.MOVE

10004

Unsigned8

Read/Write

-