AXIS#.SAFE.SCA_#.INTERNALSTATE
Description
Indicates the internal state of the Safe CAm (SCA) function state machine.
| Value | Description |
|---|---|
|
0 |
Not in range |
|
1 |
In range |
Context
For complete SCA information refer to AXIS#.SAFE.SCA_#.INTERNALSTATE.
Related safety parameters:
- AXIS#.SAFE.SCA_#.INRANGE
- AXIS#.SAFEPARAM.SCA_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SCA_#.POSLOWERLIMIT
- AXIS#.SAFEPARAM.SCA_#.POSUPPERLIMIT
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |