AXIS#.SAFEPARAM.SCA_#.FUNCTIONACTIVATION

Description

Indicates whether the Safe CAm (SCA) safety function can be activated. One of the following values is used:

Value

Description

0

Never active

2

Always activated

This function can only be used when a safe encoder is configured in the safety parameters. This function cannot be activated by using a safe input or FSoE.

Parameters Editor with the Function Activation list of values showing and all options circled

Context

For complete SCA information refer to SCA (Safe Cam).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 2

Default Value

0 (Never Active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SCA_1.FUNCTIONACTIVATION

316fh

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SCA_2.FUNCTIONACTIVATION

3170h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SCA_3.FUNCTIONACTIVATION

3171h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_1.FUNCTIONACTIVATION

326fh

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_2.FUNCTIONACTIVATION

3270h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SCA_3.FUNCTIONACTIVATION

3271h

01h

Unsigned8

-

-

Read/Write

No