AXIS#.SAFE.SLA.INTERNALSTATE
Description
Indicates the internal state of the Safely Limited Acceleration (SLA) function state machine.
| Value | Description |
|---|---|
|
0 |
Not Running |
|
1 |
Monitoring |
|
2 |
Fault Reaction |
State Machine Diagram
Context
For complete SLA information refer to SLA (Safely Limited Acceleration).
Related safety parameters:
- AXIS#.SAFE.SLA.ACTIVE
- AXIS#.SAFEPARAM.SLA.ACCLIMIT
- AXIS#.SAFEPARAM.SLA.FAULTREACTION
- AXIS#.SAFEPARAM.SLA.FSOE
- AXIS#.SAFEPARAM.SLA.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLA.SAFEINPUT
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0, 1 , 2, 3 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |