AXIS#.SAFEPARAM.SLA.FAULTREACTION

Description

Indicates the safety function activated when the Safely Limited Acceleration (SLA) safety function is faulted. The parameter can use one of the following values:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Context

For complete SLA information refer to SLA (Safely Limited Acceleration).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2 , 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLA.FAULTREACTION

3165h

05h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLA.FAULTREACTION

3265h

05h

Unsigned8

-

-

Read/Write

No