AXIS#.SAFE.SDIn.MOTIONACTIVE

Description

Indicates whether the axis is moving in the negative direction or not when Safe Direction negative (SDIn) is not active (when SDIn is active, if the axis cannot move in the negative direction, the fault reaction is activated).

Value Description

0

Not moving

1

Moving

Context

For complete SDI information refer to SDI (Safe Direction).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read Only

Units

NA

Range

0, 1

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.SDIN.MOTIONACTIVE

66dfh

01h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.SDIN.MOTIONACTIVE

6edfh

01h

Unsigned8

-

-

Read only

Yes