AXIS#.SAFE.SDIn.INTERNALSTATE
Description
Indicates the internal state of the Safe Direction negative (SDIn) function state machine.
| Value | Description |
|---|---|
|
0 |
Moving Positive Direction |
|
1 |
Stopped |
|
2 |
Delay Before Monitoring |
|
3 |
Not Running |
|
4 |
Fault Reaction |
State Machine Diagram
Context
For complete SDI information refer to SDI (Safe Direction).
Related safety parameters:
- AXIS#.SAFE.SDI.FAULTREACTION
- AXIS#.SAFE.SDIn.MOTIONACTIVE
- AXIS#.SAFE.SDIp.INTERNALSTATE
- AXIS#.SAFE.SDIp.MOTIONACTIVE
- AXIS#.SAFEPARAM.SDI.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SDI.POSZEROWINDOW
- AXIS#.SAFEPARAM.SDI.VELZEROWINDOW
- AXIS#.SAFEPARAM.SDIn.FSOE
- AXIS#.SAFEPARAM.SDIn.SAFEINPUT
- AXIS#.SAFEPARAM.SDIn.TIMEDELAYMONITORING
- AXIS#.SAFEPARAM.SDIp.FSOE
- AXIS#.SAFEPARAM.SDIp.SAFEINPUT
- AXIS#.SAFEPARAM.SDIp.TIMEDELAYMONITORING
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-00-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read only |
|
Units |
NA |
|
Range |
0, 1, 2, 3, 4 |
|
Default Value |
NA |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |