AXIS#.SAFEPARAM.SDI.FAULTREACTION

Description

Indicates the safety function activated when the Safe Direction (SDI) safety function is faulted. The parameter can take one of the following values:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Parameters Editor with all values for Fault Reaction shown and circled

Context

For complete SDI information refer to SDI (Safe Direction)

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2 , 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDI.FAULTREACTION

3164h

0ah

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDI.FAULTREACTION

3264h

0ah

Unsigned8

-

-

Read/Write

No