AXIS#.SAFE.SLI_#.ACTIVE
Description
Indicates whether the Safely Limited Increment (SLI) function instance is active.
| Value | Description |
|---|---|
|
0 |
Not active |
|
1 |
Active |
Context
For complete SLI information refer to SLI (Safely Limited Increment).
Related safety parameters:
- AXIS#.SAFEPARAM.SLI_#.FAULTREACTION
- AXIS#.SAFEPARAM.SLI_#.FSOE
- AXIS#.SAFEPARAM.SLI_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLI_#.POSRELLOWERLIMIT
- AXIS#.SAFEPARAM.SLI_#.POSRELUPPERLIMIT
- AXIS#.SAFEPARAM.SLI_#.SAFEINPUT
- AXIS#.SAFEPARAM.SLI_#.TIMEDELAYMONITORING
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFE.SLI_1.ACTIVE |
66bfh |
01h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS1.SAFE.SLI_2.ACTIVE |
66bfh |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS1.SAFE.SLI_3.ACTIVE |
66bfh |
03h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.SLI_1.ACTIVE |
6ebfh |
01h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.SLI_2.ACTIVE |
6ebfh |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |
|
AXIS2.SAFE.SLI_3.ACTIVE |
6ebfh |
03h |
Unsigned8 |
- |
- |
Read only |
Yes |