AXIS#.SAFEPARAM.SLI_#.POSRELLOWERLIMIT

Description

Indicates the relative position lower limit of the Safely Limited Increment (SLI) safety function.

 

Parameters Editor with Position Relative Lower Limit (s_LL_SLI) value circled

This is s_LL_SLI in the following diagram:

Context

For complete SLI information refer to SLI (Safely Limited Increment).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLI_1.POSRELLOWERLIMIT

3169h

06h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_2.POSRELLOWERLIMIT

316ah

06h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_3.POSRELLOWERLIMIT

316bh

06h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_1.POSRELLOWERLIMIT

3269h

06h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_2.POSRELLOWERLIMIT

326ah

06h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_3.POSRELLOWERLIMIT

326bh

06h

Unsigned32

-

-

Read/Write

No