AXIS#.SAFE.SSM_#.INRANGE

Description

Indicates whether the Safe Speed Monitor (SSM) function instance is active.

Value

Description

0

Not active

1

Active

Context

For complete SSM information refer to SSM (Safe Speed Monitor).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read Only

Units

N/A

Range

0, 1

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.SSM_1.INRANGE

66e0h

01h

Unsigned8

-

-

Read only

Yes

AXIS1.SAFE.SSM_2.INRANGE

66e0h

02h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.SSM_1.INRANGE

6ee0h

01h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.SSM_2.INRANGE

6ee0h

02h

Unsigned8

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

10080

1

10080 (0x2760)

AXIS1.SAFE.SSM_1.INRANGE

Unsigned8

Read Only

Yes

75616

2

10080 (0x2760)

AXIS2.SAFE.SSM_1.INRANGE

Unsigned8

Read Only

Yes

10081

1

10081 (0x2761)

AXIS1.SAFE.SSM_2.INRANGE

Unsigned8

Read Only

Yes

75617

2

10081 (0x2761)

AXIS2.SAFE.SSM_2.INRANGE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SAFE.SSM_1.INRANGE

10080

Unsigned8

Read Only

-

AXIS#.SAFE.SSM_2.INRANGE

10081

Unsigned8

Read Only

-