AXIS#.SAFEPARAM.ABSOLUTEPOSEN

Description

Indicates whether the absolute position support is enabled or not. If in use, the absolute position will be valid if the current value read in the encoder by the SMM matches the one stored in its non-volatile memory. If there is a mismatch, the absolute position will be marked as invalid (see AXIS#.SAFEPARAM.ABSOLUTEPOSVALID) and a safe homing will be required before using function that requires an absolute position (as SLP [Safe Limited Position]).


  • This parameter must be enabled for any functions that needs an absolute position.

Value

Description

0

Disabled

1

Enabled

 

Parameters Editor showing the Enabled setting for Absolute Position circled

Context

For safe encoder details refer to Motor feedback requirements.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Disabled)

Data Type

Integer

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.ABSOLUTEPOSEN

3150h

04h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.ABSOLUTEPOSEN

3250h

04h

Unsigned8

-

-

Read/Write

No