AXIS#.SAFEPARAM.ABSOLUTEPOSRANGE
Description
Indicates the absolute position range presented to the user. The range can be composed of unsigned values or signed values. This is only usable when a safe encoder is configured in the safety parameters and when the absolute position support is enabled (see AXIS#.SAFEPARAM.ABSOLUTEPOSEN). The SMM does not extend the position by adding software multi-turn bits. The size of the range is fixed and directly related to the encoder's number of multi-turn bits. The SMM will simply rollover the position if the encoders move outside of the pre-defined range.
Example:
If the encoder has 12 multi-turn bits then the range of absolute position multi-turn bits will be:
- Unsigned: [0,+4095]
- Signed: [-2048,+2047]
You can choose the homing value inside the range using AXIS#.SAFEPARAM.ABSOLUTEPOSRESETVALUE.
|
Value |
Description |
|---|---|
|
0 |
Unsigned range |
|
1 |
Signed range |
Context
For safe encoder details refer to Motor feedback requirements.
Related safety parameters:
- AXIS#.SAFEPARAM.ABSOLUTEPOSEN
- AXIS#.SAFEPARAM.ABSOLUTEPOSVALID
- AXIS#.SAFEPARAM.ABSOLUTEPOSRESETVALUE
- AXIS#.SAFEPARAM.ABSOLUTEPOSRESETSOURCE
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
0 (Unsigned range) |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFEPARAM.ABSOLUTEPOSRANGE |
3150h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.ABSOLUTEPOSRANGE |
3250h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |