SAFE.MONITOR#.INSTANCE
Description
Defines the instance of the monitored SMM variable returned by SAFE.MONITOR#.DATA. Two variables can be configured at the same time using SAFE.MONITOR1.INSTANCE and SAFE.MONITOR2.INSTANCE.
Code
--> SAFE.MONITOR1.INSTANCE 1
Context
Related safety parameters:
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 4 |
|
Default Value |
1 |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
N/A |