SAFE.MONITOR#.SOURCE
Description
Defines the source of the monitored safe variable SAFE.MONITOR#.DATA. Two variables can be configured at the same time using SAFE.MONITOR1.SOURCE and SAFE.MONITOR2.SOURCE. The source can be one of the following values:
|
Value |
Content |
Safety |
|---|---|---|
|
1 |
Current state of the internal state machine of the STO function |
2 and 3 |
|
2 |
Current state of the internal state machine of the SS1 function |
2 and 3 |
|
3 |
Current state of the internal state machine of the SBC function |
2 and 3 |
|
4 |
Current state of the internal state machine of the brake (Axis information is ignored, Two instances for brake 1 and 2 are provided) |
2 and 3 |
|
5 to 20 |
reserved, Functional Safety Option 3 only |
|
|
5 |
Safe position of axis |
3 |
|
6 |
Safe absolute position of axis |
3 |
|
7 |
Acceleration of axis |
3 |
|
8 |
Speed of axis |
3 |
|
9 |
Current state of the internal state machine of the SSM function |
3 |
|
10 |
Current state of the internal state machine of the SOS function |
3 |
|
11 |
Current state of the internal state machine of the SSR function |
3 |
|
12 |
Current state of the internal state machine of the SDIp function |
3 |
|
13 |
Current state of the internal state machine of the SDIn function |
3 |
|
14 |
Current state of the internal state machine of the SCA function |
3 |
|
15 |
Current state of the internal state machine of the SLA function |
3 |
|
16 |
Current state of the internal state machine of the SLS function |
3 |
|
17 |
Current state of the internal state machine of the SS2 function |
3 |
|
18 |
Current state of the internal state machine of the SLI function |
3 |
|
19 |
Current state of the internal state machine of the SLP function |
3 |
|
20 |
Current state of the internal state machine of the SAR function |
3 |
Code
--> SAFE.MONITOR1.SOURCE 2
Context
Related safety parameters:
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Read/Write |
|
Description |
Source of the monitored SMM variable |
|
Units |
N/A |
|
Range |
0 to 20 |
|
Default Value |
1 |
|
Data Type |
N/A |